Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
Hello,
I am facing an issue while transmitting continuous data via UART in TMS320F280025C microcontroller. I have referred a demo code that transmits the value 0x55 continuously, but when I checked the waveform on the oscilloscope, I couldn't see it.
I have attached a code for your reference. If there are any mistakes or issues in the code, please suggest.
Additionally, if there are specific error messages or behaviors you've observed, please share those details as well.
I am using SCIA_TX(GPIO2 for TX) and SCIA_RX(GPIO3 for RX).
//
// Included Files
//
#include "f28x_project.h"
//
// Defines
//
// Define AUTOBAUD to use the autobaud lock feature
//#define AUTOBAUD
//
// Globals
//
uint16_t loopCounter = 0;
//
// Function Prototypes
//
void initSCIAEchoback(void);
void transmitSCIAChar(uint16_t a);
void transmitSCIAMessage(unsigned char * msg);
void initSCIAFIFO(void);
//
// Main
//
void main(void)
{
uint16_t ReceivedChar;
unsigned char *msg;
//
// Initialize device clock and peripherals
//
InitSysCtrl();
//
// Initialize GPIO
//
InitGpio();
//
// For this example, only init the pins for the SCI-A port.
// GPIO_SetupPinMux() - Sets the GPxMUX1/2 and GPyMUX1/2 register bits
// GPIO_SetupPinOptions() - Sets the direction and configuration of GPIOs
// These functions are found in the F28X7x_Gpio.c file.
//
GPIO_SetupPinMux(3, GPIO_MUX_CPU1, 1);
GPIO_SetupPinOptions(3, GPIO_INPUT, GPIO_PUSHPULL);
GPIO_SetupPinMux(2, GPIO_MUX_CPU1, 1);
GPIO_SetupPinOptions(2, GPIO_OUTPUT, GPIO_ASYNC);
//
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR)
//
InitPieVectTable();
loopCounter = 0;
initSCIAEchoback(); // Initialize SCI for echoback
while(1)
{
while (SciaRegs.SCIFFTX.bit.TXFFST != 0){}
SciaRegs.SCITXBUF.all = 0x55;
}
}
//
// initSCIAEchoback - Initialize SCI-A for echoback
//
void initSCIAEchoback(void)
{
//
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function
//
SciaRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback
// No parity, 8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.all = 0x0003;
SciaRegs.SCICTL2.bit.TXINTENA = 1;
SciaRegs.SCICTL2.bit.RXBKINTENA = 1;
//
// SCIA at 9600 baud
// @LSPCLK = 12.5 MHz (50 MHz SYSCLK) HBAUD = 0x00 and LBAUD = 0xA2.
// lspclk
SciaRegs.SCIHBAUD.all = 0x0000;
SciaRegs.SCILBAUD.all = 0x00A2;
SciaRegs.SCIFFTX.all = 0xE040;
SciaRegs.SCIFFRX.all = 0x2044;
SciaRegs.SCIFFCT.all = 0x0;
SciaRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset
// SciaRegs.SCIFFRX.bit.RXFIFORESET = 1;
}
where LSPCLK to be 12.5MHz but in the demo code, it is set to 25 MHz. I am attaching the sysctrl file for your reference.
//###########################################################################
//
// FILE: f28002x_sysctrl.c
//
// TITLE: f28002x Device System Control Initialization & Support Functions.
//
// DESCRIPTION: Example initialization of system resources.
//
//###########################################################################
//
//
// $Copyright:
// Copyright (C) 2023 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "f28002x_device.h" // Headerfile Include File
#include "f28002x_examples.h" // Examples Include File
//
// Functions that will be run from RAM need to be assigned to a different
// section. This section will then be mapped to a load and run address using
// the linker cmd file.
//
// *IMPORTANT*
//
// IF RUNNING FROM FLASH, PLEASE COPY OVER THE SECTION ".TI.ramfunc" FROM
// FLASH TO RAM PRIOR TO CALLING InitSysCtrl(). THIS PREVENTS THE MCU FROM
// THROWING AN EXCEPTION WHEN A CALL TO DELAY_US() IS MADE.
//
#pragma CODE_SECTION(InitFlash, ".TI.ramfunc");
#pragma CODE_SECTION(FlashOff, ".TI.ramfunc");
// The following values are used to validate PLL Frequency using DCC
//
#define DCC_COUNTER0_TOLERANCE 1
//
// Macro used for adding delay between 2 consecutive writes to CLKSRCCTL1
// register.
// Delay = 300 NOPs
//
#define SYSCTRL_CLKSRCCTL1_DELAY asm(" RPT #250 || NOP \n RPT #50 || NOP")
//
// To use INTOSC as the clock source, comment the #define USE_PLL_SRC_XTAL,
// and uncomment the #define USE_PLL_SRC_INTOSC
//
#define USE_PLL_SRC_XTAL
//#define USE_PLL_SRC_INTOSC
//
// InitSysCtrl - Initialization of system resources.
//
void InitSysCtrl(void)
{
//
// Disable the watchdog
//
DisableDog();
#ifdef _FLASH
//
// Copy time critical code and Flash setup code to RAM. This includes the
// following functions: InitFlash()
//
// The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart
// symbols are created by the linker. Refer to the device .cmd file.
//
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
//
// Call Flash Initialization to setup flash waitstates. This function must
// reside in RAM.
//
InitFlash();
#endif
//
// Initialize the SYSPLL control to generate a 200Mhz clock
//
// Defined options to be passed as arguments to this function are defined
// in f28002x_examples.h.
//
// Note: The internal oscillator CANNOT be used as the PLL source if the
// PLLSYSCLK is configured to frequencies above 194 MHz.
//
// PLLSYSCLK = (XTAL_OSC) * (IMULT) /(REFDIV) * (ODIV) * (PLLSYSCLKDIV)
//
#if defined(USE_PLL_SRC_XTAL)
InitSysPll(XTAL_OSC, IMULT_30, REFDIV_2, ODIV_3, PLLCLK_BY_1, SYSCTL_DCC_BASE0);
#elif defined(USE_PLL_SRC_INTOSC)
InitSysPll(INT_OSC2, IMULT_30, REFDIV_1, ODIV_3, PLLCLK_BY_1, SYSCTL_DCC_BASE0);
#endif
#ifndef _FLASH
//
// Call Device_cal function when run using debugger
// This function is called as part of the Boot code. The function is called
// in the InitSysCtrl function since during debug time resets, the boot code
// will not be executed and the gel script will reinitialize all the
// registers and the calibrated values will be lost.
//
Device_cal();
#endif
//
// Turn on all peripherals
//
InitPeripheralClocks();
}
//
// InitPeripheralClocks - Initializes the clocks for the peripherals.
//
// Note: In order to reduce power consumption, turn off the clocks to any
// peripheral that is not specified for your part-number or is not used in the
// application
//
void InitPeripheralClocks(void)
{
EALLOW;
CpuSysRegs.PCLKCR0.bit.DMA = 1;
CpuSysRegs.PCLKCR0.bit.CPUTIMER0 = 1;
CpuSysRegs.PCLKCR0.bit.CPUTIMER1 = 1;
CpuSysRegs.PCLKCR0.bit.CPUTIMER2 = 1;
CpuSysRegs.PCLKCR0.bit.HRCAL = 1;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
CpuSysRegs.PCLKCR0.bit.CPUBGCRC = 1;
CpuSysRegs.PCLKCR2.bit.EPWM1 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM2 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM3 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM4 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM5 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM6 = 1;
CpuSysRegs.PCLKCR2.bit.EPWM7 = 1;
CpuSysRegs.PCLKCR3.bit.ECAP1 = 1;
CpuSysRegs.PCLKCR3.bit.ECAP2 = 1;
CpuSysRegs.PCLKCR3.bit.ECAP3 = 1;
CpuSysRegs.PCLKCR4.bit.EQEP1 = 1;
CpuSysRegs.PCLKCR4.bit.EQEP2 = 1;
CpuSysRegs.PCLKCR7.bit.SCI_A = 1;
CpuSysRegs.PCLKCR8.bit.SPI_A = 1;
CpuSysRegs.PCLKCR8.bit.SPI_B = 1;
CpuSysRegs.PCLKCR9.bit.I2C_A = 1;
CpuSysRegs.PCLKCR10.bit.CAN_A = 1;
CpuSysRegs.PCLKCR13.bit.ADC_A = 1;
CpuSysRegs.PCLKCR13.bit.ADC_C = 1;
CpuSysRegs.PCLKCR14.bit.CMPSS1 = 1;
CpuSysRegs.PCLKCR14.bit.CMPSS2 = 1;
CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1;
CpuSysRegs.PCLKCR14.bit.CMPSS4 = 1;
CpuSysRegs.PCLKCR19.bit.LIN_A = 1;
CpuSysRegs.PCLKCR19.bit.LIN_B = 1;
CpuSysRegs.PCLKCR20.bit.PMBUS_A = 1;
CpuSysRegs.PCLKCR21.bit.DCC0 = 1;
CpuSysRegs.PCLKCR21.bit.DCC1 = 1;
EDIS;
}
//
// DisablePeripheralClocks - Gates-off all peripheral clocks.
//
void DisablePeripheralClocks(void)
{
EALLOW;
CpuSysRegs.PCLKCR0.all = 0;
CpuSysRegs.PCLKCR2.all = 0;
CpuSysRegs.PCLKCR3.all = 0;
CpuSysRegs.PCLKCR4.all = 0;
CpuSysRegs.PCLKCR7.all = 0;
CpuSysRegs.PCLKCR8.all = 0;
CpuSysRegs.PCLKCR9.all = 0;
CpuSysRegs.PCLKCR10.all = 0;
CpuSysRegs.PCLKCR13.all = 0;
CpuSysRegs.PCLKCR14.all = 0;
CpuSysRegs.PCLKCR19.all = 0;
CpuSysRegs.PCLKCR20.all = 0;
CpuSysRegs.PCLKCR21.all = 0;
EDIS;
}
//
// InitFlash - This function initializes the Flash Control registers.
//
// *CAUTION*
// This function MUST be executed out of RAM. Executing it out of OTP/Flash
// will yield unpredictable results.
//
#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#endif
void InitFlash(void)
{
EALLOW;
//
// At reset bank and pump are in sleep. A Flash access will power up the
// bank and pump automatically.
//
// Power up Flash bank and pump. This also sets the fall back mode of
// flash and pump as active.
//
Flash0CtrlRegs.FPAC1.bit.PMPPWR = 0x1;
Flash0CtrlRegs.FBFALLBACK.bit.BNKPWR0 = 0x3;
//
// Disable Cache and prefetch mechanism before changing wait states
//
Flash0CtrlRegs.FRD_INTF_CTRL.bit.DATA_CACHE_EN = 0;
Flash0CtrlRegs.FRD_INTF_CTRL.bit.PREFETCH_EN = 0;
//
// Set waitstates according to frequency
//
// *CAUTION*
// Minimum waitstates required for the flash operating at a given CPU rate
// must be characterized by TI. Refer to the datasheet for the latest
// information.
//
#if CPU_FRQ_100MHZ
Flash0CtrlRegs.FRDCNTL.bit.RWAIT = 0x4;
#endif
//
// Enable Cache and prefetch mechanism to improve performance of code
// executed from Flash.
//
Flash0CtrlRegs.FRD_INTF_CTRL.bit.DATA_CACHE_EN = 1;
Flash0CtrlRegs.FRD_INTF_CTRL.bit.PREFETCH_EN = 1;
//
// At reset, ECC is enabled. If it is disabled by application software and
// if application again wants to enable ECC.
//
Flash0EccRegs.ECC_ENABLE.bit.ENABLE = 0xA;
EDIS;
//
// Force a pipeline flush to ensure that the write to the last register
// configured occurs before returning.
//
__asm(" RPT #7 || NOP");
}
//
// FlashOff - This function powers down the flash
//
// *CAUTION*
// This function MUST be executed out of RAM. Executing it out of OTP/Flash
// will yield unpredictable results. Also you must seize the flash pump in
// order to power it down.
//
#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#endif
void FlashOff(void)
{
EALLOW;
//
// Power down bank
//
Flash0CtrlRegs.FBFALLBACK.bit.BNKPWR0 = 0;
//
// Power down pump
//
Flash0CtrlRegs.FPAC1.bit.PMPPWR = 0;
EDIS;
}
//
// ServiceDog - This function resets the watchdog timer.
//
// Enable this function for using ServiceDog in the application.
//
void ServiceDog(void)
{
EALLOW;
WdRegs.WDKEY.bit.WDKEY = 0x0055;
WdRegs.WDKEY.bit.WDKEY = 0x00AA;
EDIS;
}
//
// DisableDog - This function disables the watchdog timer.
//
void DisableDog(void)
{
volatile Uint16 temp;
//
// Grab the clock config first so we don't clobber it
//
EALLOW;
temp = WdRegs.WDCR.all & 0x0007;
WdRegs.WDCR.all = 0x0068 | temp;
EDIS;
}
//
// InitPll - This function initializes the PLL registers.
//
// Note: This function uses the DCC to check that the PLLRAWCLK is running at
// the expected rate. The desirable DCC can be provided as a parameter.
//
void InitSysPll(Uint16 clock_source, Uint16 imult, Uint32 refdiv, Uint32 odiv,
Uint16 divsel, Uint32 dccbase)
{
Uint32 timeout,temp_syspllmult, pllLockStatus;
bool status;
if(((clock_source & 0x3) == ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL) &&
(((clock_source & 0x4) >> 2) == ClkCfgRegs.XTALCR.bit.SE) &&
(imult == ClkCfgRegs.SYSPLLMULT.bit.IMULT) &&
(refdiv == ClkCfgRegs.SYSPLLMULT.bit.REFDIV) &&
(odiv == ClkCfgRegs.SYSPLLMULT.bit.ODIV) &&
(divsel == ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV))
{
//
// Everything is set as required, so just return
//
return;
}
EALLOW;
//
// First modify the PLL multipliers if the multipliers need an update or PLL needs
// to be powered on / enabled
//
if((imult != ClkCfgRegs.SYSPLLMULT.bit.IMULT) ||
(refdiv != ClkCfgRegs.SYSPLLMULT.bit.REFDIV)||
(odiv != ClkCfgRegs.SYSPLLMULT.bit.ODIV) ||
(1U != ClkCfgRegs.SYSPLLCTL1.bit.PLLEN))
{
//
// Bypass PLL and set dividers to /1
//
ClkCfgRegs.SYSPLLCTL1.bit.PLLCLKEN = 0;
//
// Delay of at least 120 OSCCLK cycles required post PLL bypass
//
asm(" RPT #120 || NOP");
//
// Evaluate PLL multipliers and dividers
//
temp_syspllmult = ((refdiv << 24U) | (odiv << 16U)| imult);
//
// Turnoff the PLL
//
ClkCfgRegs.SYSPLLCTL1.bit.PLLEN = 0;
EDIS;
//
// Delay of at least 66 OSCCLK cycles
//
asm(" RPT #66 || NOP");
if(((clock_source & 0x3) != ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL) ||
(((clock_source & 0x4) >> 2) != ClkCfgRegs.XTALCR.bit.SE))
{
switch (clock_source)
{
case INT_OSC1:
SysIntOsc1Sel();
break;
case INT_OSC2:
SysIntOsc2Sel();
break;
case XTAL_OSC:
SysXtalOscSel();
break;
case XTAL_OSC_SE:
SysXtalOscSESel();
break;
}
}
//
// Delay of at least 60 OSCCLK cycles
//
asm(" RPT #60 || NOP");
EALLOW;
//
// Set dividers to /1 to ensure the fastest PLL configuration
//
ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = 0;
//
// Program PLL multipliers
//
ClkCfgRegs.SYSPLLMULT.all = temp_syspllmult;
//
// Enable SYSPLL
//
ClkCfgRegs.SYSPLLCTL1.bit.PLLEN = 1;
//
// Lock time is 1024 OSCCLK * (REFDIV+1)
//
timeout = (1024U * (refdiv + 1U));
pllLockStatus = ClkCfgRegs.SYSPLLSTS.bit.LOCKS;
//
// Wait for the SYSPLL lock
//
while((pllLockStatus != 1) && (timeout != 0U))
{
pllLockStatus = ClkCfgRegs.SYSPLLSTS.bit.LOCKS;
timeout--;
}
EDIS;
//
// Check PLL Frequency using DCC
//
status = IsPLLValid(dccbase, clock_source, INT_PLL_SYSPLL,
imult, odiv , refdiv);
}
else
{
//
// Re-Lock of PLL not needed since the multipliers
// are not updated
//
status = true;
}
if(status)
{
EALLOW;
//
// Set divider to produce slower output frequency to limit current increase
//
if(divsel != PLLCLK_BY_126)
{
ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = divsel + 1;
}
else
{
ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = divsel;
}
//
// Enable PLLSYSCLK is fed from system PLL clock
//
ClkCfgRegs.SYSPLLCTL1.bit.PLLCLKEN = 1;
//
// Small 100 cycle delay
//
asm(" RPT #100 || NOP");
//
// Set the divider to user value
//
ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = divsel;
EDIS;
}
else
ESTOP0; // If the frequency is out of range, stop here.
}
//
// SysIntOsc1Sel - This function switches to Internal Oscillator 1.
//
void SysIntOsc1Sel(void)
{
EALLOW;
ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL = 2; // Clk Src = INTOSC1
EDIS;
}
//
// SysIntOsc2Sel - This function switches to Internal oscillator 2.
//
void SysIntOsc2Sel(void)
{
EALLOW;
ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL = 0; // Clk Src = INTOSC2
EDIS;
}
//
// PollX1Counter - Clear the X1CNT counter and then wait for it to saturate
// four times.
//
static void
PollX1Counter(void)
{
Uint16 loopCount = 0;
//
// Delay for 1 ms while the XTAL powers up
//
// 2000 loops, 5 cycles per loop + 9 cycles overhead = 10009 cycles
//
F28x_usDelay(2000);
//
// Clear and saturate X1CNT 4 times to guarantee operation
//
do
{
//
// Keep clearing the counter until it is no longer saturated
//
while(ClkCfgRegs.X1CNT.all > 0x1FF)
{
ClkCfgRegs.X1CNT.bit.CLR = 1;
ClkCfgRegs.X1CNT.bit.CLR = 0;
}
//
// Wait for the X1 clock to saturate
//
//
// while(ClkCfgRegs.X1CNT.all != 0x7FFU)
// {
// ;
// }
//
// Increment the counter
//
loopCount++;
}while(loopCount < 4);
}
// SysXtalOscSel - This function switches to External CRYSTAL oscillator.
//
void SysXtalOscSel(void)
{
EALLOW;
ClkCfgRegs.XTALCR.bit.OSCOFF = 0; // Turn on XTALOSC
ClkCfgRegs.XTALCR.bit.SE = 0; // Select crystal mode
EDIS;
//
// Wait for the X1 clock to saturate
//
PollX1Counter();
//
// Select XTAL as the oscillator source
//
EALLOW;
ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL = 1;
EDIS;
//
// If a missing clock failure was detected, try waiting for the X1 counter
// to saturate again. Consider modifying this code to add a 10ms timeout.
//
while(ClkCfgRegs.MCDCR.bit.MCLKSTS != 0)
{
EALLOW;
ClkCfgRegs.MCDCR.bit.MCLKCLR = 1;
EDIS;
//
// Wait for the X1 clock to saturate
//
PollX1Counter();
//
// Select XTAL as the oscillator source
//
EALLOW;
ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL = 1;
EDIS;
}
}
//
// SysXtalOscSESel - This function switches to external oscillator in
// single-ended mode and turns off all other clock sources to minimize power
// consumption. This option may not be available on all device packages
//
void
SysXtalOscSESel (void)
{
EALLOW;
ClkCfgRegs.XTALCR.bit.OSCOFF = 0; // Turn on XTALOSC
ClkCfgRegs.XTALCR.bit.SE = 1; // Select single-ended mode
EDIS;
//
// Wait for the X1 clock to saturate
//
PollX1Counter();
//
// Select XTALOSC as the oscillator source
//
EALLOW;
ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL = 1;
EDIS;
//
// If missing clock detected, there is something wrong with the oscillator
// module.
//
if(ClkCfgRegs.MCDCR.bit.MCLKSTS != 0)
{
ESTOP0;
}
}
//
// IDLE - Enter IDLE mode
//
void
IDLE()
{
EALLOW;
CpuSysRegs.LPMCR.bit.LPM = LPM_IDLE;
EDIS;
asm(" IDLE");
}
//
// HALT - Enter HALT mode
//
void
HALT()
{
EALLOW;
CpuSysRegs.LPMCR.bit.LPM = LPM_HALT;
ClkCfgRegs.SYSPLLCTL1.bit.PLLCLKEN = 0;
ClkCfgRegs.SYSPLLCTL1.bit.PLLEN = 0;
EDIS;
asm(" IDLE");
}
//*****************************************************************************
//
// SysCtl_isPLLValid()
//
//*****************************************************************************
bool
IsPLLValid(Uint32 base, Uint16 oscSource, Uint16 pllclk, Uint16 imult,
Uint16 odiv, Uint16 refdiv)
{
float fclk1_0ratio;
volatile struct DCC_REGS *DccRegs;
EALLOW;
//
// Assigning DCC for PLL validation
// Enable Peripheral Clock Domain PCLKCR21 for DCC
//
if(base == SYSCTL_DCC_BASE0)
{
DccRegs = &Dcc0Regs;
CpuSysRegs.PCLKCR21.bit.DCC0 = 1;
}
else if(base == SYSCTL_DCC_BASE1)
{
DccRegs = &Dcc1Regs;
CpuSysRegs.PCLKCR21.bit.DCC1 = 1;
}
else
ESTOP0; // Invalid DCC selected
//
// Clear Error & Done Flag
//
DccRegs->DCCSTATUS.bit.ERR = 1;
DccRegs->DCCSTATUS.bit.DONE = 1;
//
// Disable DCC
//
DccRegs->DCCGCTRL.bit.DCCENA = 0x5;
//
// Disable Error Signal
//
DccRegs->DCCGCTRL.bit.ERRENA = 0x5;
//
// Disable Done Signal
//
DccRegs->DCCGCTRL.bit.DONEENA = 0x5;
//
// Configure Clock Source1 to PLL
//
// Clk Src1 Key 0xA to enable clock source selection
//
switch(pllclk)
{
case INT_PLL_SYSPLL:
DccRegs->DCCCLKSRC1.all = 0xA000; // Clk Src1 = SYSPLL
break;
default:
//
// Code shouldn't reach here
//
break;
}
//
// Configure Clock Source0 to whatever is set as a reference
// clock source for PLL
//
// Clk Src0 Key 0xA to enable clock source selection
//
switch(oscSource)
{
case INT_OSC1:
DccRegs->DCCCLKSRC0.all = 0xA001; // Clk Src0 = INTOSC1
break;
case INT_OSC2:
DccRegs->DCCCLKSRC0.all = 0xA002; // Clk Src0 = INTOSC2
break;
case XTAL_OSC:
case XTAL_OSC_SE:
DccRegs->DCCCLKSRC0.all = 0xA000; // Clk Src0 = XTAL
break;
default:
//
// Code shouldn't reach here
//
break;
}
//
// Calculating frequency ratio of output clock(f1) vs reference clock(f0)
//
fclk1_0ratio = (float)imult / ((odiv + 1U) * (refdiv + 1));
//
// Computing and configuring Counter0 , Counter1 & Valid Seed Values
// with +/-1% tolerance for the desired DCC
//
ComputeCntrSeedValue(base, fclk1_0ratio, DCC_COUNTER0_TOLERANCE);
//
// Enable Single Shot Mode
//
DccRegs->DCCGCTRL.bit.SINGLESHOT = 0xA;
//
// Enable DCC to start counting
//
DccRegs->DCCGCTRL.bit.DCCENA = 0xA;
EDIS;
//
// Wait until Error or Done Flag is generated
//
while((DccRegs->DCCSTATUS.all & 3) == 0)
{
}
//
// Returns true if DCC completes without error
//
return((DccRegs->DCCSTATUS.all & 3) == 2);
}
//*****************************************************************************
//
// ComputeCntSeedValid - Compute Counter seed values based on the frequency ratio of output
// clock vs reference clock & tolerance expected for the desired DCC
//
//*****************************************************************************
void ComputeCntrSeedValue(Uint32 base, float fclk1_0ratio, Uint32 tolerance)
{
Uint32 window, dccCounterSeed0, dccValidSeed0, dccCounterSeed1, total_error;
volatile struct DCC_REGS *DccRegs;
if(fclk1_0ratio >= 1U)
{
//
// Setting Counter0 & Valid Seed Value with expected tolerance
// Total error is 12
//
window = (12U * 100U) / tolerance;
dccCounterSeed0 = window - 12U;
dccValidSeed0 = 24U;
}
else
{
total_error = (((Uint32)2U / fclk1_0ratio) + (Uint32)10U);
window = ((total_error * 100U)/ tolerance);
//
// Setting Counter0 & Valid Seed Value with expected tolerance
//
dccCounterSeed0 = window - total_error;
dccValidSeed0 = (Uint32)2U * total_error;
}
//
// Multiplying Counter-0 window with PLL Integer Multiplier
//
dccCounterSeed1 = window * fclk1_0ratio;
//
// Assigning DCC for PLL validation
//
if(base == SYSCTL_DCC_BASE0)
DccRegs = &Dcc0Regs;
else if(base == SYSCTL_DCC_BASE1)
DccRegs = &Dcc1Regs;
else
ESTOP0; // Invalid DCC selected
//
// Configure COUNTER-0, COUNTER-1 & Valid Window
//
DccRegs->DCCCNTSEED0.bit.COUNTSEED0 = dccCounterSeed0; // Loaded Counter0 Value
DccRegs->DCCVALIDSEED0.bit.VALIDSEED = dccValidSeed0; // Loaded Valid Value
DccRegs->DCCCNTSEED1.bit.COUNTSEED1 = dccCounterSeed1; // Loaded Counter1 Value
}
//
// End of File
//