Other Parts Discussed in Thread: OPA320, THS4531
Hi,
I am using hall based current sensor ACS725LLCTR-30AB-T in my design and the supply voltage given to it is 3.3V(Single ended).
The input current is +-24A sinusoidal and the HALL IC is shifting the output to 1.65V, hence the output swing I am getting is 0 to 3.3V(Full current swing) radiometric with supply.
Please find below image for reference circuit.
Previously I was using single ended ADC of TMS320F28377DPTPEP, for current sensing so directly given the output of OPA320 buffer stage to the ADC along with filter.
Now I wanted to use a differential 16bit ADC of microcontroller.
I am planning to use THS4531 diff Amplifier, with the single ended input range 0 to 3V.
What should be supply voltage given to THS4531 to +VS and -VS pin, and also the VOCM pin highlighted in yellow.
The VREFHI=3V and VREFLO=0V in current design, do we need to change that to VREFHI=1.5V ?
Please provide your inputs so that I could get an idea for starting the design.
Thanks,
Namita