Part Number: TMS320F28377D
#cpu1
int main(void)
{
Device_init();
g_stCpu1RWBaseInfo.ulCpu1BootStatus = *((uint32_t *)0x0000002C);
#cpu2
void main(void)
{
Device_init();
g_stCpu2RWBaseInfo.ulCpu2BootStatus = *((uint32_t *)0x00000002);
Interrupt_initModule();
process:CPU1 start running,CPU2 start running,and CPU2 enable wdg,after 10s,stop feed wdg,then both cpu1 and cpu2 reset;
read cpu1BootStatus is 0x00004F00,cpu2BootStatus is 0x80000d00;
1、why do not tell me reset infomation about wdg from bootStatus?
2、when debug,it will enter CPU1 NMI interrupt,so why do not tell me infomation about nmi from bootStatus?
--
Thanks & Regards