Part Number: TMS320F28069
Hello,
I am running 4 TMS320F28069 devices in connection. The debugger is "XDS200 JTAG Emulator". I created a target configuration on CCS ver 12.4.0.00007. I created with the graphic user interface as the picture attached. The ccxml source code is generated automatically. In the source code of the file, I am expecting there should be 4 device tags but there is only 3. Although I see there are 4 device description for TMS320F28069_x, it looks one of the device information is simplified. Can you help explaining on this?
Thanks,
Andy

<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS2xx USB Debug Probe_0">
<instance XML_version="1.2" desc="Texas Instruments XDS2xx USB Debug Probe_0" href="connections/TIXDS2XXUSB_Connection.xml" id="Texas Instruments XDS2xx USB Debug Probe_0" xml="TIXDS2XXUSB_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS2xx USB Debug Probe_0">
<instance XML_version="1.2" href="drivers/tixds560c28x.xml" id="drivers" xml="tixds560c28x.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560cla.xml" id="drivers" xml="tixds560cla.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320F28069_0" href="devices/f28069.xml" id="TMS320F28069_0" xml="f28069.xml" xmlpath="devices"/>
<instance XML_version="1.2" desc="TMS320F28069_1" href="devices/f28069.xml" id="TMS320F28069_1" xml="f28069.xml" xmlpath="devices"/>
<device HW_revision="1" XML_version="1.2" description="" id="TMS320F28069_1" partnum="TMS320F28069">
<cpu HW_revision="1.0" XML_version="1.2" desc="C28xx_0" description="CPU" id="C28xx_0" isa="TMS320C28XX"/>
<cpu HW_revision="1.0" XML_version="1.2" desc="CLA_1" description="CLA Accelerator" id="CLA_0" isa="TMS192C2006"/>
</device>
<instance XML_version="1.2" desc="TMS320F28069_2" href="devices/f28069.xml" id="TMS320F28069_2" xml="f28069.xml" xmlpath="devices"/>
<device HW_revision="1" XML_version="1.2" description="" id="TMS320F28069_2" partnum="TMS320F28069">
<cpu HW_revision="1.0" XML_version="1.2" desc="C28xx_1" description="CPU" id="C28xx_0" isa="TMS320C28XX"/>
<cpu HW_revision="1.0" XML_version="1.2" desc="CLA_2" description="CLA Accelerator" id="CLA_0" isa="TMS192C2006"/>
</device>
<instance XML_version="1.2" desc="TMS320F28069_3" href="devices/f28069.xml" id="TMS320F28069_3" xml="f28069.xml" xmlpath="devices"/>
<device HW_revision="1" XML_version="1.2" description="" id="TMS320F28069_3" partnum="TMS320F28069">
<cpu HW_revision="1.0" XML_version="1.2" desc="C28xx_2" description="CPU" id="C28xx_0" isa="TMS320C28XX"/>
<cpu HW_revision="1.0" XML_version="1.2" desc="CLA_3" description="CLA Accelerator" id="CLA_0" isa="TMS192C2006"/>
</device>
</platform>
</connection>
</configuration>
</configurations>