Part Number: TMS320F280049C
Other Parts Discussed in Thread: TIDM-1000, , SFRA
Hi Ti Team,
I'm using 3phase Vienna rectifier TIDM-1000 with TMS320F280049C controller.
This board is designed for,
1. Three-Phase Input 208 VL-L 60 Hz, Output 600-V
DC Nominal, 1.2 KW
2. Three-Phase Input 400 VL-L 50 Hz, Output 700-V
DC Nominal, 2.4 KW
As per my understanding, here we are using SFRA to check system stability.
Is SFRA used in this design applicable only evaluation boards?
If it's not, can I use this SFRA for my custom board?
which is designed for,
Three-Phase Input 400 VL-L 50 Hz, Output 900-V
DC Nominal, 6 KW.