Other Parts Discussed in Thread: CONTROLSUITE
Dear all,
I'm confuse about coeffieient of Multiplier, the user guid tell me the Multiplier is the weighting factor used in exponential moving average.
We use MATH_EMAVG marco to get the average value of AC Line, the Multiplier value for this can be estimated through Time Domain as below:
Our sampling at 100KHz and the input AC signal is 60Hz. as the average of the rectified sine signal is desired the effective frequency of the signal being averaged is 120Hz. the implies that (100KHz/120)=833 samples in one half sine. so we can get Multiplier for 1/833=0.0012.
but why user guid calculation is 1/3332=0.003 and tell me AC line average a value of 4000 samples (it averages roughly over 4 sine halves) in DPLib.pdf page 120?
Another, in Frequency Domain section, why the cut-off frequency is 5Hz? if our Frequency use 50Hz, what's the cut-off frequency?