This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-XDS110: dimensions

Expert 6760 points
Part Number: LP-XDS110


hi, I am looking for dimensinons e.g. hole positions, 20-pin position, USB-C position. And/or an STP model. Can you help?

  • Hi,

    You can use the design files for the Energy Trace version of the LP-XDS110 for this: 

    LP-XDS110-ET (SPRR479): https://www.ti.com/lit/zip/sprr479 

    The only difference will be that the Energy Trace components are removed; the dimensions are the same. The PCB design files are design using Cadence Allegro, so they are in that format. There are also generated Gerber files included, which can be used for finding the PCB dimensions.

    Regards,

    Zack