Part Number: TIDM-1000
Hi Team,
Here're some issues from the customer may need your help:
1. In the VIENN rectifier, is the inductor behind the current transformer used for filtering?
2. The maximum input current written in the manual is 4A, so what is the current after passing through the current transformer? If the load is different, what is the maximum current through the inductor?
3. Can you provide a detailed schematic diagram of the current transformer?
--
Thanks & Regards