This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: CMPSS module

Part Number: TMS320F2800137

Hi expert:

   

The functions of the comparator are as follows: when the input voltage(cmp0_hp) is greater than the set value (2V, using internal DAC), it outputs a high level,Output through XBAR-7

At present, the input voltage is 0v. When initializing CMPSS module, a high level of 30 ns will appear,why?

Did the comparator output become erratic during the internal DAC power on process after CMPSS_enablemodule?