Part Number: TMS320F2800157-Q1
Hi experts,
my customer is now using F2800157 and is using internal oscillator as clock source of F2800157.
He has the following questions:
1. Which internal oscillator is better for the clock source? The customer is now using INTOSC1.
2. What are the risks if the clock that is not recommended is used?
From TRM I know that INTOSC2 is used to run the boot ROM and can be used as the system clock source for the application. INTOSC1 is a backup clock source that normally only clocks the watchdog timers and missing clock detection circuit (MCD). But I don't know which one would be better.
Thanks!
Best Regards
Kita