Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi,
I cannot connect the device, attached an image/
What is the reason.
in the device manager it looks like it identify the connection:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi,
I cannot connect the device, attached an image/
What is the reason.
in the device manager it looks like it identify the connection:

Hello Ben,
Without using GUI composer, can you try to use the target configurations file (ccxml) to connect with the device by itself? If there are no errors, try to launch the selected target configuration and see what shows up in the console. Make sure the connection is secure and the board is properly powered (you can use a multimeter on the JTAG pins to confirm the voltages are at the right levels).
Hello Ben,
To verify what is causing this issue, please use the default CCS and try connecting via the target configurations file by itself; if the same CCS version on both operating systems has this same result, then let me know so I can forward this to the CCS experts.
Import an example from C2000Ware or other project example, try to connect to the board using the target configurations file without using GUI composer. Essentially, don't use GUI composer and see if you still have an issue.