Part Number: TMS320F28069F
Other Parts Discussed in Thread: LAUNCHXL-F28069M
Hello TI team,
We are using LAUNCHXL-F28069M for CAN implementation.
There is a problem, there no data on the can bus when we check the signal on the Oscilloscope.
Below is the code that i used for.
Thanks
Nitish Sharma
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
//
// Function Prototypes
//
void mailbox_check(int32 T1, int32 T2, int32 T3);
void mailbox_read(int16 i);
//
// Globals
//
Uint32 ErrorCount;
Uint32 PassCount;
Uint32 MessageReceivedCount;
Uint32 TestMbox1 = 0;
Uint32 TestMbox2 = 0;
Uint32 TestMbox3 = 0;
//
// Main
//
void main(void)
{
Uint16 j;
//
// eCAN control registers require read/write access using 32-bits. Thus we
// will create a set of shadow registers for this example. These shadow
// registers will be used to make sure the access is 32-bits and not 16.
//
struct ECAN_REGS ECanaShadow;
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2806x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initalize GPIO:
// This example function is found in the F2806x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
// InitGpio(); // Skipped for this example
//
// For this example, configure CAN pins using GPIO regs here
// This function is found in F2806x_ECan.c
//
InitECanGpio();
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2806x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2806x_DefaultIsr.c.
// This function is found in F2806x_PieVect.c.
//
InitPieVectTable();
//
// Step 4. Initialize all the Device Peripherals:
// This function is found in F2806x_InitPeripherals.c
//
// InitPeripherals(); // Not required for this example
//
// Step 5. User specific code, enable interrupts:
//
MessageReceivedCount = 0;
ErrorCount = 0;
PassCount = 0;
InitECana(); // Initialize eCAN-A module
//
// Mailboxs can be written to 16-bits or 32-bits at a time
// Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15
//
ECanaMboxes.MBOX0.MSGID.all = 0x9555AAA0;
//
// Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31
//
ECanaMboxes.MBOX16.MSGID.all = 0x9555AAA0;
// Configure Mailboxes 0-15 as Tx, 16-31 as Rx
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
//
ECanaRegs.CANMD.all = 0xFFFF0000;
//
// Enable all Mailboxes
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
//
ECanaRegs.CANME.all = 0xFFFFFFFF;
//
// Specify that 8 bits will be sent/received
//
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
// Write to the mailbox RAM field of MBOX0 - 15
//
ECanaMboxes.MBOX0.MDL.all = 0x11111111;
ECanaMboxes.MBOX0.MDH.all = 0xFFFFFFFF;
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
//
EALLOW;
ECanaRegs.CANMIM.all = 0xFFFFFFFF;
//
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
//
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.STM = 0; // 1 for self-test mode, 0 for external
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
EDIS;
//
// Begin transmitting
//
for(;;)
{
//
// Set TRS for all transmit mailboxes
//
ECanaRegs.CANTRS.all = 0x0000FFFF;
// Wait for all TAn bits to be set
while(ECanaRegs.CANTA.all != 0x0000FFFF )
{
}
ECanaRegs.CANTA.all = 0x0000FFFF; // Clear all TAn
for (int i=0; i<1000; i++);
}
}
//
// mailbox_read - This function reads out the contents of the indicated
// by the Mailbox number (MBXnbr). MSGID of a rcv MBX is transmitted as the
// MDL data.
//
void
mailbox_read(int16 MBXnbr)
{
volatile struct MBOX *Mailbox;
Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
TestMbox3 = Mailbox->MSGID.all; // = 0x9555AAAn (n is the MBX number)
}
//
// mailbox_check -
//
void
mailbox_check(int32 T1, int32 T2, int32 T3)
{
if((T1 != T3) || ( T2 != 0x89ABCDEF))
{
ErrorCount++;
}
else
{
PassCount++;
}
}