Other Parts Discussed in Thread: C2000WARE
Hi community,
I'm working on EEPROM 1 byte write and read using I2C polling method inspired by "i2c_ex2_eeprom" and "i2c_ex4_eeprom_polling" examples of C2000Ware SDK
I tried to run examples of both codes I could not write to or read from the AT24XX breakup board.
So I tried with the below code without bus_scan() with the existing library i2cLib_FIFO_polling in the i2c_ex4_eeprom_polling example
can you help me with the flow to configure write and read from the EEPROM
as per my information acquired from the SDK following functions are called in the order please check an update if necessary
To i2c master function call flow:
I2C_setDataCount();
I2C_setConfig();
I2C_setAddressMode();
I2C_setTargetAddress();
I2C_putData();
I2C_sendStartCondition();
// wait for Tx/Rx data
I2C_sendStopCondition();
Here I attached the code made as simple as possible after this also I'm not able to write or read data from the EEPROM
#include "driverlib.h"
#include "device.h"
#include "i2cLib_FIFO_polling.h"
//
// Defines
//
#define EEPROM_ADDR 0x50
//
// Globals
//
struct I2CHandle EEPROM;
uint16_t TX_MsgBuffer[MAX_BUFFER_SIZE];
uint16_t RX_MsgBuffer[MAX_BUFFER_SIZE];
uint32_t ControlAddr;
uint16_t status;
void I2C_GPIO_init(void)
{
// I2CA pins (SDAA / SCLA)
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SDAA, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SDAA, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SDAA, GPIO_QUAL_ASYNC);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCLA, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCLA, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCLA, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SDAA);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCLA);
}
void I2Cinit(void)
{
//myI2CA initialization
I2C_disableModule(I2CA_BASE);
I2C_initController(I2CA_BASE, DEVICE_SYSCLK_FREQ, 100000, I2C_DUTYCYCLE_50);
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_SEND_MODE);
I2C_setTargetAddress(I2CA_BASE, 0x50);
// I2C_setOwnAddress(I2CA_BASE, 96); //I2CA address
I2C_disableLoopback(I2CA_BASE);
I2C_setBitCount(I2CA_BASE, I2C_BITCOUNT_8);
I2C_setDataCount(I2CA_BASE, 2);
I2C_setAddressMode(I2CA_BASE, I2C_ADDR_MODE_7BITS);
I2C_enableFIFO(I2CA_BASE);
I2C_clearInterruptStatus(I2CA_BASE, I2C_INT_ARB_LOST | I2C_INT_NO_ACK);
I2C_setFIFOInterruptLevel(I2CA_BASE, I2C_FIFO_TXEMPTY, I2C_FIFO_RX2);
I2C_enableInterrupt(I2CA_BASE, I2C_INT_ADDR_TARGET | I2C_INT_ARB_LOST | I2C_INT_NO_ACK | I2C_INT_STOP_CONDITION);
I2C_setEmulationMode(I2CA_BASE, I2C_EMULATION_FREE_RUN);
I2C_enableModule(I2CA_BASE);
}
//
// pass - Function to be called if data written matches data read
//
void
pass(void)
{
asm(" ESTOP0");
for(;;);
}
//
// fail - Function to be called if data written does NOT match data read
//
void fail(void)
{
asm(" ESTOP0");
for(;;);
}
void verifyEEPROMRead(void)
{
uint16_t i;
while(I2C_getStatus(I2CA_BASE) & I2C_STS_BUS_BUSY);
for(i=0;i<EEPROM.NumOfDataBytes;i++)
{
if(RX_MsgBuffer[i] != TX_MsgBuffer[i])
{
//Transmitted data doesn't match received data
//Fail condition. PC shouldn't reach here
ESTOP0;
fail();
}
}
}
//
// Main
//
void main()
{
volatile int status = 0;
uint16_t i;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize I2C pins
//
I2C_GPIO_init();
//
// Initialize PIE and clear PIE registers. Disable CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
I2Cinit();
EEPROM.TargetAddr = 0x50;
EEPROM.base = I2CA_BASE;
EEPROM.pControlAddr = &ControlAddr;
EEPROM.NumOfAddrBytes = 2;
EEPROM.pTX_MsgBuffer = TX_MsgBuffer;
EEPROM.pRX_MsgBuffer = RX_MsgBuffer;
EEPROM.NumOfAttempts = 5;
EEPROM.Delay_us = 10;
EEPROM.WriteCycleTime_in_us = 6000; //10ms for EEPROM this code was tested
//Example 1: EEPROM Byte Write
//Write 11 to EEPROM address 0x0
ControlAddr = 0x01;
EEPROM.NumOfDataBytes = 1;
TX_MsgBuffer[0] = 11;
status = I2C_ControllerTransmitter(&EEPROM);
//Wait for EEPROM write cycle time
//This delay is not mandatory. User can run their application code instead.
//It is however important to wait for EEPROM write cycle time before you initiate
//another read / write transaction
DEVICE_DELAY_US(EEPROM.WriteCycleTime_in_us);
//Example 2: EEPROM Byte Read
//Make sure 11 is written to EEPROM address 0x0
ControlAddr = 0x01;
EEPROM.pControlAddr = &ControlAddr;
EEPROM.NumOfDataBytes = 1;
status = I2C_ControllerReceiver(&EEPROM);
while(I2C_getStatus(EEPROM.base) & I2C_STS_BUS_BUSY);
verifyEEPROMRead();
}
correct me if I'm wrong anywhere looking forward to solutions or hints.
In TRM
"START and STOP conditions can be generated by the I2C module when the module is configured to be a master on the I2C bus."
Q. After which instruction we can observe CLOCK and DATA on the DSO?.
In my case not able to view SCL and SDA for any of the example programs immediately after "void I2Cinit(void)" and "I2C_sendStartCondition(base);" these functions.
Q. Give general steps for I2C debugging from both software and hardware perspective for any TI board.
Thanks and regards,
Ajaykumar V