Part Number: TMS320F280039C
Other Parts Discussed in Thread: TIDA-010062
Hi Team,
My customer is using TIDA-010062 and want to load program to flash. The bode mode remain high state during power up and boot stage.
We referenced the 3.1.5.4 Loading the Custom Bootloader and Application to Flash Using CCS of this manual:
https://www.ti.com/lit/ug/tiduet7g/tiduet7g.pdf
There is no Bank0_LDFU and Bank1_LDFU in the ttplpfc f28003x file.
How should the customer add it to the project? If added directly, the compilation will report an error.

It can be selected in the imported flash_kernel_ex3_sci_flash_kernel project.
Do we need to use this program to configure the mcu first?

--
Thanks & Regards