Other Parts Discussed in Thread: CODECOMPOSER
Hi!
I have the following issue:
I load the program I want to debug in flash. When I start a new debug session in CodeComposer I can connect to the board, the program is running, but I cannot read any variable. Is there something else I must do besides connecting to the target? in the window where I connect to the target I always get two debug session, and no matter in which I do the connect target, the program runs after a reset but I can't read the variables.
If I start the debug session by re-flashing I can read the variables, but this is very slow, especially because when I try to flash the second time, CodeComposer does not respond anymore, I must close it and start it again, sometimes I have to restart the computer also. I've reinstalled CodeComposer but didn't help...
Can somebody help me with this?
Thanks,
Monica