Work environment:The servo driver is equipped with a 17-bit Tamagawa encoder.My client has a lot of on-site interference.
My client has a lot of on-site interference.It is often found that the data returned by the encoder cannot be received and the alarm is raised
Test:
The EFT is 5K and 100K, respectively, and the amplitude is 4000V,which can cause problems at the customer site.We tested the encoder when something went wrong, and it returned data.
We should receive the 11 bytes of data, but ScibRegs. SCIFFRX. Bit. RXFFST shows received their number is 0/1/3,If we debug directly to ScibRegs SCICTL1. SWRESET 0, 1, again. So cibRegs SCIFFRX. Bit. RXFFST will work properly.
The problem:
Is it the interference that causes the SCI of 280039 to work abnormally? Or has SCI stopped working?
Why does this happen?
Is there any good way to solve it? Be in a hurry
EFT

Customer


Debug