Hi Trey,
I am trying to use this flash linker file without success. Is there a switch I have to turn on in CSS to make the change from RAM to Flash?
Here's a snapshot of my memory map:
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
CSM_ECSL_Z1 00200000 00000030 00000000 00000030 RWIX
FLASH 00200030 0007ffa0 00000000 0007ffa0 R X
CSM_ECSL_Z2 0027ffd0 00000030 00000000 00000030 RWIX
C0 20000000 00002000 00000000 00002000 RW X
C1 20002000 00002000 00000624 000019dc RW X
BOOT_RSVD 20004000 00000ff8 00000000 00000ff8 R X
RESETISR 20004ff8 00000008 00000006 00000002 RW X
INTVECS 20005000 000001b0 000001b0 00000000 RW X
C2 200051b0 00000e50 000004b4 0000099c RW X
C3 20006000 00002000 00000000 00002000 RW X
S0 20008000 00002000 00000000 00002000 RW X
S1 2000a000 00002000 00000000 00002000 RW X
S2 2000c000 00002000 00000000 00002000 RW X
S3 2000e000 00002000 00000000 00002000 RW X
S4 20010000 00002000 00000000 00002000 RW X
S5 20012000 00002000 00000000 00002000 RW X
S6 20014000 00002000 00000000 00002000 RW X
S7 20016000 00002000 00000000 00002000 RW X
CTOMRAM 2007f000 00000800 00000000 00000800 R X
MTOCRAM 2007f800 00000800 00000000 00000800 RW X
Thanks,
Tim