This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: (Error -1156 @ 0xB677) Device may be operating in low-power mode.

Part Number: TMS320F28377D

Hi. I'm encountering an issue while using the TMS320F28377D processor. I'm not receiving the clock output despite using an external oscillator of 20MHz. I'm using CCS 10 and XDS100V2 Emulator. When I run the program, it shows an error message - "device is operating in low power mode." I've monitored the voltage levels and found them to be satisfactory. I've included the ti-c2000 sysctrl.c file without any modifications. The configuration is set as follows: XTAL_OSC, IMULT_20, FMULT_0, PLLCLK_BY_2. Any insights or suggestions would be greatly appreciated.