Part Number: TMS320F28388D
Hi Experts,
Customer use F28388D to achieve ADC 16bit mode single-ended sampling Voltage. We find that ADC sampling error very larger below:
ADC VREFHIA-D voltage is 3.0V, ADC analog Pin input Voltage/single-ended is 0~3.0V. We test different voltage on analog Pin/B2/B3. there are very larger error between actual and theoretical values.

You can see the below customer's code. they use S/W trigger SOC signal on B2/B3 pin.


In addition, we eliminate the influence of memory cross talk, modify the above code, and only retain B2 per SOC for ADC sampling. we found that there is still a large deviation between the actual value and the theoretical value.
When Voltage = 2.546V,ADC Result value is 53750,but the theoretical values is 55617.
When Voltage = 2.349V,ADC Result value is 49520,but the theoretical values is 51313.
Could you help us review code and some suggestion/Dir? Thanks.