Part Number: TIDM-1000
Hi,
In the Vienna rectifier code, memory mapping is done for Control code ISR and Instrumentation ISR as shown below using sections "isrcodefuncs" and "ramfuncs".
If I want to write ADC ISR how should I do the memory mapping. Can I use same " isrcodefuncs " , for defining any other interrupt like ADC?
Or should I define a new section in the CMD file.
---------------------------------------------------------------------------------------------------------
#if VIENNA_CONTROL_RUNNING_ON == C28x_CORE
#ifndef __TMS320C28XX_CLA__
#pragma INTERRUPT (ISR1, HPI)
#pragma CODE_SECTION(ISR1,"isrcodefuncs");
interrupt void ISR1(void);
#endif
#else
#endif
#if VIENNA_INSTRUMENTATION_ISR_RUNNING_ON == C28x_CORE
#ifndef __TMS320C28XX_CLA__
#pragma CODE_SECTION(ISR2,"ramfuncs");
interrupt void ISR2(void);
#endif
#else
#endif
----------------------------------------------------------------------------------------------------------------
Thanks and Regards,
Neeraja