Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE
Dear Champs,
I am asking this for our customer.
They found even they use -O2 (optimization level) for such simple C codes like
Pseudo codes below:
int16 X[7]
int16 A[7]
int32 Y
Y = X[0]A[0] + X[1]A[1] + X[2]A[2] + X[3]A[3] + X[4]A[4] + X[5]A[5] + X[6]A[6] // These code are running from RAM.
But the found the result is still around 0.5 us. (using 120-MHz F280039C CPU)
They are asking if there is any better way to write fast C code without assembly.
Do you have any suggestion?
I notice our FIR16 : Y= a[i]x[i] (Y in int32 and a, x in int16) in
C:\ti\c2000\C2000Ware_5_01_00_00\libraries\dsp\FixedPoint\c28\docs
Can this be viewed as very fast codes for this kind of multiply-accumulation-based codes?
Is calling TI FIR16 library is the only way we suggest or do you have any better idea?