Hello,
I am currently designing a control system based on the TMS320F28386D microcontroller. It has to control two different inverters simultaneously.
In addition, each inverter has an interleaving configuration, so I need to sinchronize the operation. For that purpose, I have to take out two different EXTSYNCOUT signals.
I want to know if taking out two EXTSYNCOUTSIGNAL via GPIO is possible, and if it is possible how it can be configured.
By the figure 17-6 of the TMS320F2838x manual, it appears that only one EXTSYNCOUT signal can be routed from the ePWM module to OUTPUT X-BAR GPIO.

Thanks in advance,
Daniel Pérez