Part Number: TMS320F2800137
Hi expert:
In Technical Reference Manual
Describe 1:
5.7.8 Device Unique ID
TI OTP contains a 256-bit value that is made up of both random and sequential parts. This value can be used as a seed for code encryption. The starting address of the value is 0x7020E. The first 192 bits are random, the next 32 bits are sequential, and the last 32 bits are a checksum value
Describe 2:
Table 3-19. SYSCTRL Base Address Table
UidRegs UID_REGS UID_BASE Base Address:0x0007_1140
why address is different?
which address is the right ?