Hi Team,
There's an issue from the customer need your help:
TIDM-02010—dmpfc-0013X's dual motor code, I only want to use this code to control one motor, I configure the underlying configuration of motor 1 (ADC sampling, PWM wave, etc.) as my chip requirements, in which PFC and motor 2 bottom configuration have not been changed; Then the test was carried out, following the dual motors
In the manual "Dual Motor Control Reference Design for HVAC with Digital Interleaved PFC", Motor 1 was able to emit the set PWM wave when the first part of the CPU and board settings were completed, but when the V/F test was performed, the motor voltage and current were too small to start the motor rotation. Is there a more detailed description of the test documentation? Among them, I have confirmed that there is basically no problem with ADC sampling, the relay is also smoothly closed when it is powered on, and when performing the V/F test, the motor also emits a duty cycle, but the motor cannot rotate, please explain, what parameters need to be modified. Thank you
Best Regards,
Ben