Part Number: TMS320F28388D
Hi champs,
In EtherCAT application, my customer would like to know is it possible to force Ethernet PHY DP83822 enters power down mode by using F28388D software API?
Please advise your comments, thanks.
Regards,
Luke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Hi champs,
In EtherCAT application, my customer would like to know is it possible to force Ethernet PHY DP83822 enters power down mode by using F28388D software API?
Please advise your comments, thanks.
Regards,
Luke
Discussion moved offline. Suggestions provided:
Believe this is possible by writing to PHY register BMCR bit[11] and maybe also DPDWN bit[2] if they want to go into Deep Power Down.


If you need PHY register read / write functions using MII interface you can leverage the functions below. Note that these functions are for the C28 core, slightly modified functions would be needed for CM core (8-bit byte addressable).
Function Declarations:
//
// Functions for reading / writing to DP838xx PHY devices
//
#define ESC_MII_CTRL_STATUS_OFFSET 0x0510 // 0x288 - Low
#define ESC_PHY_ADDRESS_OFFSET 0x0512 // 0x289 - Low
#define ESC_PHY_REG_ADDRESS_OFFSET 0x0513 // 0x289 - High
#define ESC_PHY_DATA_OFFSET 0x0514 // 0x28A - Low
#define ESC_MII_ECAT_ACCESS_OFFSET 0x0516 // 0x28B - Low
#define ESC_MII_PDI_ACCESS_OFFSET 0x0517 // 0x28B - High
//
// Function for reading from an ESC PHY register using CPU1 -
// Assumes Word and address are 16-bit values
//
uint16_t mii_readPhyRegister(uint16_t address, uint16_t target_phy_address)
{
// Set PHY address to read/write, (0x0513//0x289 HIGH byte)
ESC_writeWordISR((address<<8) | target_phy_address, ESC_PHY_ADDRESS_OFFSET);
// Write PHY reg, (0x0510//0x288 low)
ESC_writeWordISR(0x0103,ESC_MII_CTRL_STATUS_OFFSET);
while(ESC_readWordISR(ESC_MII_CTRL_STATUS_OFFSET) != 0x3); // wait till read is completed and successful
return ESC_readWordISR(ESC_PHY_DATA_OFFSET);
}
//
// Function for writing to an ESC PHY register using CPU1 -
// Assumes Word and address are 16-bit values
//
void mii_writePhyRegister(uint16_t address, uint16_t target_phy_address, uint16_t data)
{
// Set PHY address to read/write, (0x0513//0x289 HIGH byte)
ESC_writeWordISR((address<<8) | target_phy_address, ESC_PHY_ADDRESS_OFFSET);
ESC_writeWordISR(data, ESC_PHY_DATA_OFFSET);
ESC_writeWordISR(0x203, ESC_MII_CTRL_STATUS_OFFSET);
while(ESC_readWordISR(ESC_MII_CTRL_STATUS_OFFSET) != 0x3); // wait till write is completed and successful
}
//
// Function for reading from an Extended ESC PHY register using CPU1 -
// Assumes Word and address are 16-bit values
//
uint16_t mii_readPhyExtendedRegister(uint16_t address, uint16_t target_phy_address)
{
mii_writePhyRegister(0xD, target_phy_address, 0x1F); //Phy reg 0xD = 0x1F
mii_writePhyRegister(0xE, target_phy_address, address); //Phy Reg 0xE = *Address of register outside of 0-1F
mii_writePhyRegister(0xD, target_phy_address, 0x401F); //Phy reg 0xD = 0x401F
return(mii_readPhyRegister(0xE,target_phy_address)); // Extended read data
}
void enable_PDI_access_to_MII(void)
{
ESC_writeWordISR(0x0100,ESC_MII_ECAT_ACCESS_OFFSET); // Give PDI access to MII management
return;
}
uint16_t phy_regs_0[32]; // For storing first 32 PHY registers of Port0
uint16_t ext_phy_regs_0[48]; // For storing Extended PHY registers of Port0
uint16_t phy_regs_1[32]; // For storing first 32 PHY registers of Port1
uint16_t ext_phy_regs_1[48]; // For storing Extended PHY registers of Port1
Usage of Functions:
//
// Initialize ESCSS Memory
//
ESCSS_initMemory(ESC_SS_BASE);
//
// Wait for ESCSS memory initialization to complete
//
if(ESCSS_getMemoryInitDoneStatusBlocking(ESC_SS_BASE, memoryTimeOut) !=
ESCSS_API_SUCCESS)
{
return(ESC_HW_INIT_FAIL);
}
ESTOP0;
// Read PHY registers...
enable_PDI_access_to_MII();
DEVICE_DELAY_US(100);
uint16_t index;
//
// Read Port0 PHY Registers
//
// Read first 32 PHY registers (non-extended)
for (index = 0; index < 32; ++index)
{
phy_regs_0[index] = mii_readPhyRegister(index, 0x00);
}
DEVICE_DELAY_US(100);
// Read extended PHY registers
ext_phy_regs_0[0] = mii_readPhyRegister(0x25, 0x00);
ext_phy_regs_0[1] = mii_readPhyRegister(0x27, 0x00);
ext_phy_regs_0[2] = mii_readPhyRegister(0x2A, 0x00);
ext_phy_regs_0[3] = mii_readPhyRegister(0x117, 0x00);
ext_phy_regs_0[4] = mii_readPhyRegister(0x131, 0x00);
ext_phy_regs_0[5] = mii_readPhyRegister(0x170, 0x00);
ext_phy_regs_0[6] = mii_readPhyRegister(0x171, 0x00);
ext_phy_regs_0[7] = mii_readPhyRegister(0x173, 0x00);
ext_phy_regs_0[8] = mii_readPhyRegister(0x175, 0x00);
ext_phy_regs_0[9] = mii_readPhyRegister(0x176, 0x00);
ext_phy_regs_0[10] = mii_readPhyRegister(0x177, 0x00);
ext_phy_regs_0[11] = mii_readPhyRegister(0x178, 0x00);
ext_phy_regs_0[12] = mii_readPhyRegister(0x180, 0x00);
ext_phy_regs_0[13] = mii_readPhyRegister(0x181, 0x00);
ext_phy_regs_0[14] = mii_readPhyRegister(0x182, 0x00);
ext_phy_regs_0[15] = mii_readPhyRegister(0x183, 0x00);
ext_phy_regs_0[16] = mii_readPhyRegister(0x184, 0x00);
ext_phy_regs_0[17] = mii_readPhyRegister(0x185, 0x00);
ext_phy_regs_0[18] = mii_readPhyRegister(0x186, 0x00);
ext_phy_regs_0[19] = mii_readPhyRegister(0x187, 0x00);
ext_phy_regs_0[20] = mii_readPhyRegister(0x188, 0x00);
ext_phy_regs_0[21] = mii_readPhyRegister(0x189, 0x00);
ext_phy_regs_0[22] = mii_readPhyRegister(0x18A, 0x00);
ext_phy_regs_0[23] = mii_readPhyRegister(0x302, 0x00);
ext_phy_regs_0[24] = mii_readPhyRegister(0x303, 0x00);
ext_phy_regs_0[25] = mii_readPhyRegister(0x304, 0x00);
ext_phy_regs_0[26] = mii_readPhyRegister(0x305, 0x00);
ext_phy_regs_0[27] = mii_readPhyRegister(0x306, 0x00);
ext_phy_regs_0[28] = mii_readPhyRegister(0x308, 0x00);
ext_phy_regs_0[29] = mii_readPhyRegister(0x30B, 0x00);
ext_phy_regs_0[30] = mii_readPhyRegister(0x30C, 0x00);
ext_phy_regs_0[31] = mii_readPhyRegister(0x30E, 0x00);
ext_phy_regs_0[32] = mii_readPhyRegister(0x404, 0x00);
ext_phy_regs_0[33] = mii_readPhyRegister(0x40D, 0x00);
ext_phy_regs_0[34] = mii_readPhyRegister(0x456, 0x00);
ext_phy_regs_0[35] = mii_readPhyRegister(0x460, 0x00);
ext_phy_regs_0[36] = mii_readPhyRegister(0x461, 0x00);
ext_phy_regs_0[37] = mii_readPhyRegister(0x467, 0x00);
ext_phy_regs_0[38] = mii_readPhyRegister(0x468, 0x00);
ext_phy_regs_0[39] = mii_readPhyRegister(0x469, 0x00);
ext_phy_regs_0[40] = mii_readPhyRegister(0x4A0, 0x00);
ext_phy_regs_0[41] = mii_readPhyRegister(0x4A1, 0x00);
ext_phy_regs_0[42] = mii_readPhyRegister(0x4A2, 0x00);
ext_phy_regs_0[43] = mii_readPhyRegister(0x4A3, 0x00);
ext_phy_regs_0[44] = mii_readPhyRegister(0x4A4, 0x00);
ext_phy_regs_0[45] = mii_readPhyRegister(0x4A5, 0x00);
ext_phy_regs_0[46] = mii_readPhyRegister(0x4A6, 0x00);
ext_phy_regs_0[47] = mii_readPhyRegister(0x4A7, 0x00);
//
// Read Port1 PHY Registers
//
// Read first 32 PHY registers (non-extended)
for (index = 0; index < 32; ++index)
{
phy_regs_1[index] = mii_readPhyRegister(index, 0x01);
}
DEVICE_DELAY_US(100);
// Read extended PHY registers
ext_phy_regs_1[0] = mii_readPhyRegister(0x25, 0x01);
ext_phy_regs_1[1] = mii_readPhyRegister(0x27, 0x01);
ext_phy_regs_1[2] = mii_readPhyRegister(0x2A, 0x01);
ext_phy_regs_1[3] = mii_readPhyRegister(0x117, 0x01);
ext_phy_regs_1[4] = mii_readPhyRegister(0x131, 0x01);
ext_phy_regs_1[5] = mii_readPhyRegister(0x170, 0x01);
ext_phy_regs_1[6] = mii_readPhyRegister(0x171, 0x01);
ext_phy_regs_1[7] = mii_readPhyRegister(0x173, 0x01);
ext_phy_regs_1[8] = mii_readPhyRegister(0x175, 0x01);
ext_phy_regs_1[9] = mii_readPhyRegister(0x176, 0x01);
ext_phy_regs_1[10] = mii_readPhyRegister(0x177, 0x01);
ext_phy_regs_1[11] = mii_readPhyRegister(0x178, 0x01);
ext_phy_regs_1[12] = mii_readPhyRegister(0x180, 0x01);
ext_phy_regs_1[13] = mii_readPhyRegister(0x181, 0x01);
ext_phy_regs_1[14] = mii_readPhyRegister(0x182, 0x01);
ext_phy_regs_1[15] = mii_readPhyRegister(0x183, 0x01);
ext_phy_regs_1[16] = mii_readPhyRegister(0x184, 0x01);
ext_phy_regs_1[17] = mii_readPhyRegister(0x185, 0x01);
ext_phy_regs_1[18] = mii_readPhyRegister(0x186, 0x01);
ext_phy_regs_1[19] = mii_readPhyRegister(0x187, 0x01);
ext_phy_regs_1[20] = mii_readPhyRegister(0x188, 0x01);
ext_phy_regs_1[21] = mii_readPhyRegister(0x189, 0x01);
ext_phy_regs_1[22] = mii_readPhyRegister(0x18A, 0x01);
ext_phy_regs_1[23] = mii_readPhyRegister(0x302, 0x01);
ext_phy_regs_1[24] = mii_readPhyRegister(0x303, 0x01);
ext_phy_regs_1[25] = mii_readPhyRegister(0x304, 0x01);
ext_phy_regs_1[26] = mii_readPhyRegister(0x305, 0x01);
ext_phy_regs_1[27] = mii_readPhyRegister(0x306, 0x01);
ext_phy_regs_1[28] = mii_readPhyRegister(0x308, 0x01);
ext_phy_regs_1[29] = mii_readPhyRegister(0x30B, 0x01);
ext_phy_regs_1[30] = mii_readPhyRegister(0x30C, 0x01);
ext_phy_regs_1[31] = mii_readPhyRegister(0x30E, 0x01);
ext_phy_regs_1[32] = mii_readPhyRegister(0x404, 0x01);
ext_phy_regs_1[33] = mii_readPhyRegister(0x40D, 0x01);
ext_phy_regs_1[34] = mii_readPhyRegister(0x456, 0x01);
ext_phy_regs_1[35] = mii_readPhyRegister(0x460, 0x01);
ext_phy_regs_1[36] = mii_readPhyRegister(0x461, 0x01);
ext_phy_regs_1[37] = mii_readPhyRegister(0x467, 0x01);
ext_phy_regs_1[38] = mii_readPhyRegister(0x468, 0x01);
ext_phy_regs_1[39] = mii_readPhyRegister(0x469, 0x01);
ext_phy_regs_1[40] = mii_readPhyRegister(0x4A0, 0x01);
ext_phy_regs_1[41] = mii_readPhyRegister(0x4A1, 0x01);
ext_phy_regs_1[42] = mii_readPhyRegister(0x4A2, 0x01);
ext_phy_regs_1[43] = mii_readPhyRegister(0x4A3, 0x01);
ext_phy_regs_1[44] = mii_readPhyRegister(0x4A4, 0x01);
ext_phy_regs_1[45] = mii_readPhyRegister(0x4A5, 0x01);
ext_phy_regs_1[46] = mii_readPhyRegister(0x4A6, 0x01);
ext_phy_regs_1[47] = mii_readPhyRegister(0x4A7, 0x01);
ESTOP0;
Best,
Kevin
Edit: Updating functions to fix port1 access