Part Number: TMS320F280049C
Other Parts Discussed in Thread: LAUNCHXL-F280049C,
Hi,
I am working on developing a CAN custom bootloader to update the firmware. I am able to write to flash using this program by loading bootloader to RAM through JTAG and default S2 switch positions on LAUNCHXL-F280049C board . But I am getting CAN bus heavy/CAN bus off error if I load the custom bootloader using CAN ROM bootloader. I am using default boot pins (i.e. PIN 32 and 33 ) and CAN defaults (i.e. CANH is 33 and CANL is 32). I see a conflict b/w default boot pins and CANL using same PIN (i.e. PIN 32). How to handle this if I want to use the default boot settings and not custom one since I don't want to use OTP as of now.
Also I want to know if on request, TI supports loading our custom bootloader into ROM in factory itself?
Thanks in Advance
Mohan