Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi,
It is said that "The secure boot feature is applicable only on Zone1 and hence the chosen flash sector(s) have to be configured as Zone1-EXEONLY." in the "Secure BOOT on C2000 Device" Application Report Table 4-1
I did not understand relation between "Secure Boot" and configuring "ZONE1-EXEONLY" .
For example my application resides in sector 0. Application size only 13KB.
If I want to use "Secure Flash Boot" mode, am I have to configure flash sector 0 as EXEONLY ?
Thanks.