Other Parts Discussed in Thread: ADS1601
Hello,
I have the ADS1601/02 EVM. In its user’s guide ( SLAU147 ), it says there is an example project running in the CCSv3.3 environment, by the name ‘ADS1601-XXXX.pjt' , where the XXXX in the project’s name, stands for one of the following platforms: 5510, 6711, 6713, 6416 (from the C5000 or C6000 family). I tried to find this example project in TI’s site but couldn’t. I would really appreciate some help in finding it! I realize this is the C2000 forum but actualy i need to run this example project on the F28335, so if someone knows a similar project for the 'delfino' it would be even better.
Many thanks in advance!
Ilia