Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Hi,
I have been using tms320f28335 for close loop PI control of load current.For that i have written a code,but i am getting error messages in DCLF32.h header file.
I have attached the code and the error messages.
Kindly provide the solution and confirm weather the issue is with the code or in DCL header structure.
#include "DSP28x_Project.h"
// Device Headerfile and Examples Include File
#include "DCL.h"
#include "DSP2833x_Device.h"
#include "DSP2833x_Examples.h"
#include "DSP2833x_GlobalPrototypes.h"
#include "DCLF32.h"
#include "DCL_fdlog.h"
//#include "DCLC28.h"
#include "math.h"
//
// Function Prototypes
//
float rk = 20.0f;
float yk;
float lk;
float uk;
float Duty;
struct dcl_pi pi1;
DCL_PI pi1 = PI_DEFAULTS;
//
// Function Prototypes
//
Uint16 LoopCount;
Uint16 ConversionCount;
void adc_isr(void);
void gpio_select(void);
void InitAdc(void);
void InitEPwm1(void);
void control_Isr(void);
float DCL_runPI_C1(DCL_PI *p, float rk, float yk);
float voltage1;
float cmpa;
//
// Main
//
void main(void)
{
InitSysCtrl();
DINT;
InitPieCtrl();
EALLOW;
#if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT
//
// HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz
//
#define ADC_MODCLK 0x3
#endif
#if (CPU_FRQ_100MHZ)
//
// HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2) = 25.0 MHz
//
#define ADC_MODCLK 0x2
#endif
EDIS;
EALLOW;
SysCtrlRegs.HISPCP.all = ADC_MODCLK;
EDIS;
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.ADCINT = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
InitAdc (); // For this example, init the ADC
//gpio_select();
// InitEPwm1();
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
IER |= M_INT1;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
LoopCount = 0;
ConversionCount = 0;
/* initialise controller variables */
pi1.Kp=2.0f;
pi1.Ki=1.0f;
pi1.Umax=0.8f;
pi1.Umin=0.2f;
rk = 20.0f; // initial value for control reference
lk = 1.0f; // control loop not saturated
//
// Enable SOCA from ePWM to start SEQ1
//
// control loop not saturated
AdcRegs.ADCMAXCONV.all = 0x0001; // Setup 2 conv's on SEQ1
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x3; // Setup ADCINA3 as 1st SEQ1 conv.
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x2; // Setup ADCINA2 as 2nd SEQ1 conv.
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS)
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.half.CMPA = 1875; // Set compare A value
EPwm1Regs.TBPRD = 3750; // Set period for ePWM1
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start
for (;;)
{
LoopCount++;
}
}
//
// cpu_timer0_isr -
void gpio_select()
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0; // Enable pullup on GPIO0
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pullup on GPIO0
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = PWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO0 = PWM1B
EDIS;
}
void InitEPwm1()
{
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Count up down
EPwm1Regs.TBPRD = 3750; // Set timer period
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0x001; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = 000;
EPwm1Regs.TBCTL.bit.SYNCOSEL=1;
EPwm1Regs.CMPA.half.CMPA =1875; // Set compare A value
EPwm1Regs.CMPB = 1875; // Set Compare B value
EPwm1Regs.CMPCTL.bit.LOADAMODE=1;
EPwm1Regs.CMPCTL.bit.SHDWAMODE=0;
/* EPwm1Regs.DBCTL.bit.OUT_MODE=3;
EPwm1Regs.DBCTL.bit.POLSEL=2;
EPwm1Regs.DBCTL.bit.IN_MODE=0;
EPwm1Regs.DBRED=100;
EPwm1Regs.DBFED=100;*/
EPwm1Regs.AQCTLA.bit.ZRO=2; // Set PWM1A on Zero
EPwm1Regs.AQCTLA.bit.CAU=1;
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 1; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
}
__interrupt void adc_isr(void)
{
yk=((int)AdcRegs.ADCRESULT0 >>4)*300.0f/4095.0f;
//Voltage2[ConversionCount] = AdcRegs.ADCRESULT1 >>4;
//DCL_runClamp_C1(float *data, float Umax, float Umin);
//
lk=0.0f;
uk = DCL_runPI_C1(&pi1, rk, yk);
if (uk>0.8f){
uk=0.8f;
}
else if (uk<0.1f){
uk=0.1f;
}
//uk=0.5f;
EPwm1Regs.CMPA.half.CMPA =(EPwm1Regs.TBPRD)*uk; // Set compare A value
EPwm1Regs.CMPB = EPwm1Regs.TBPRD*uk; // Set Compare B value
// If 40 conversions have been logged, start over
//
//
// Reinitialize for next ADC sequence
//
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}
ERROR:
>> Compilation failure
subdir_rules.mk:72: recipe for target 'Example_2833xAdcSoc.obj' failed
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 146: error: expected an expression
v = DCL_DISABLE_INTS;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 173: error: struct "dcl_css" has no field "sts"
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 173: error: expected an expression
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 175: error: expected an expression
v = DCL_DISABLE_INTS;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 261: error: expected a ";"
{
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 323: error: expected a ";"
{
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 430: error: expected an expression
v = DCL_DISABLE_INTS;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 458: error: struct "dcl_pi2" has no field "css"
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 458: error: expected an expression
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 460: error: expected an expression
v = DCL_DISABLE_INTS;
^
^
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 555: error: expected an expression
v = DCL_DISABLE_INTS;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 568: error: struct "dcl_df11" has no field "css"
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 568: error: expected an expression
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 570: error: expected an expression
v = DCL_DISABLE_INTS;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 590: error: identifier "bool" is undefined
static inline bool DCL_isStableDF11(DCL_DF11 *p)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 641: error: struct "dcl_df11" has no field "css"
p->sps->b0 = Kp * (Ki * p->css->T + 2.0f) / 2.0f;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 642: error: struct "dcl_df11" has no field "css"
p->sps->b1 = Kp * (Ki * p->css->T - 2.0f) / 2.0f;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 733: error: expected an expression
v = DCL_DISABLE_INTS;
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 746: error: struct "dcl_df13" has no field "css"
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 746: error: expected an expression
if (p->css->sts & STS_UPDATE_PENDING)
^
"C:/ti/c2000/C2000Ware_4_03_00_00/libraries/control/DCL/c28/include/DCLF32.h",
line 748: error: expected an expression
v = DCL_DISABLE_INTS;
^
21 errors detected in the compilation of "../Example_2833xAdcSoc.c".
gmake: *** [Example_2833xAdcSoc.obj] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****