Hi Team,
There's an issue from the customer need your help:
On TRM 1582 pages, chapter 10.3.2.5 THIS CHAPTER IS THE ANAREFTRIMA REGISTER, WHERE ITS <10-6> BITS ARE THE FIELD BGSLOPETRIM FUNCTION, WHICH IS ADJUSTED FOR THE BANDGAP SLOPE.
where 00 - no adjustment, other values - adjustment
Excuse me, how did you adjust it? For example, if the value is "01", what is the adjusted value? Is it positive or negative?
Field < 5-0> BGVALTRIM is the same as above. Thanks for the answer.

Best Regards,
Ben