Part Number: TMS320F280039C
Other Parts Discussed in Thread: TIDA-010062, , SFRA
Hi,
When using the examples procedure of TIDA-010062,TMS320F280039C can run in debug or flash mode after emulator programing. But after the auxiliary power off, then power on again, the program is not running. Every time i power on again, i need to be reprogramming with emulator.

This is the memory allocation when using flash to program, it seems running in flash mode? And i'm sure the boot mode is flash mode (GPIO32 and GPIO24 are pulled up by 3.3V).
The following is the procedure i use.
Please help to answer this question, thank you!