Hello,
I need to generate PWM where the frequency is fixed at 20 kHz, and the duty cycle varies. The oscilloscope displays pulses at 20 kHz. However, I consistently observe a 50 percent duty cycle on the oscilloscope. Although I intended to set the duty cycle to 70 percent, the oscilloscope consistently shows a 50 percent duty cycle.
for 70 percent duty cycle I have initialize following values in code:-
#define EPWM2_TIMER_TBPRD 312 // Period register
#define EPWM2_MAX_CMPA 218
#define EPWM2_MIN_CMPA 94
#define EPWM_CMP_UP 1
#define EPWM_CMP_DOWN 0
I have attached code for your ref:-
//
// Included Files
//
#include "F28x_Project.h"
#include "common.h"
#include "extern.h"
// Globals
//
uint16_t sensorSample = 0;
uint16_t isrCount = 0;
int16_t sensorTemp = 0;
float ADC_Voltage=0;
float ADC_Voltage1=0;
float Pressure_kpa=0;
float Pressure_mbar=0;
typedef struct
{
volatile struct EPWM_REGS *EPwmRegHandle;
Uint16 EPwm_CMPA_Direction;
Uint16 EPwmTimerIntCount;
Uint16 EPwmMaxCMPA;
Uint16 EPwmMinCMPA;
}EPWM_INFO;
EPWM_INFO epwm2_info;
//
// Function Prototypes
//
void InitEPwm2Example(void);
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
//
InitSysCtrl();
//
// Initialize GPIO
//
InitGpio();
//
// enable PWM2 to drive motor..
//'
CpuSysRegs.PCLKCR2.bit.EPWM2=1;
//
// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
// These functions are in the F2837xD_EPwm.c file
//
InitEPwm2Gpio();
//
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
InitPieVectTable();
//
// For this example, only initialize the ePWM
///******************************/
// for now GPIO-3 is used for PWM signal..20khz PWM signal is generated.
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
InitEPwm2Example();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
while(1)
{
}
}
void InitEPwm2Example()
{
//
// Setup TBCLK
//
EPwm2Regs.TBPRD = EPWM2_TIMER_TBPRD; // Set timer period 801 TBCLKs
EPwm2Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter
//
// Set Compare values
//
EPwm2Regs.CMPA.bit.CMPA = EPWM2_MIN_CMPA; // Set compare A value
//
// Setup counter mode
//
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up and down
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV2; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV2;
//
// Setup shadowing
//
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
//
// Set actions
//
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM2A on event A, up
// count
EPwm2Regs.AQCTLA.bit.CBD = AQ_CLEAR; // Clear PWM2A on event B, down
// count
EPwm2Regs.AQCTLB.bit.ZRO = AQ_CLEAR; // Clear PWM2B on zero
EPwm2Regs.AQCTLB.bit.PRD = AQ_SET; // Set PWM2B on period
//
// Interrupt where we will change the Compare Values
//
EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm2Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event
//
// Information this example uses to keep track
// of the direction the CMPA/CMPB values are
// moving, the min and max allowed values and
// a pointer to the correct ePWM registers
//
epwm2_info.EPwm_CMPA_Direction = EPWM_CMP_UP; // Start by increasing CMPA
epwm2_info.EPwmTimerIntCount = 0; // Zero the interrupt counter
epwm2_info.EPwmRegHandle = &EPwm2Regs; // Set the pointer to the
// ePWM module
epwm2_info.EPwmMaxCMPA = EPWM2_MAX_CMPA; // Setup min/max CMPA/CMPB
// values
epwm2_info.EPwmMinCMPA = EPWM2_MIN_CMPA;
}