This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: getting error while i dumped code into microcontroller

Part Number: TMS320F28386D

       i am getting error while i am trying to dumped  programme and i dumped ccs code example and i am using customised microcontroller TMS320F28386D Please help me as soon as possible 

  • Hello,

    Please make sure that the device is properly powered. If you're using a ControlCARD, make sure that you have selected the correct power source for the base board (note that there is an option for USB power or external power source). You can also refer to details of setting up the ControlCARD here.