Part Number: TMS320F28027
Other Parts Discussed in Thread: MOTORWARE
Hello,
I use D:\ti\motorware\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\boostxldrv8305_revA\f28x\f2802xF\projects\ccs\proj_lab10a
GMotorVars.OverModulation is set to 0.55. I found that at 30V, the highest duty cycle of PWM reached 96%, and it was running normally, and the speed was also improved. However, when the voltage was 40v, the highest duty cycle of PWM reached 96%, and the speed was also improved, but the operation was abnormal, and it was found that the phase current fluctuated and there was abnormal noise.
1. Ask if the configuration of what is interrupted is too small, resulting in no time to deal with it. Because 30V, the maximum speed is 2300rpm,40V, and the maximum speed is 3000rpm.
2 or the phase current accuracy is not enough,