Part Number: TMS320F280037
Other Parts Discussed in Thread: C2000WARE
Hi,
Newby here i''m used to PIC's but changed jobs and they are using texas micros. We have a dev board which i am bringing to life. I'm running latest CCS and have C2000Ware5.1 installed aswell.
I have got running the PWM , the SPI. but for some reason i cannot get the MCAN to transmit other than 150kbps , which is a weird speed. We have an external clock for the CAN @ 20Mhz but i've also tried the sysclk divided down.
To check i have a CAN X-analyser and a logic analyser on the CAN-TX coming out the micro
I've used the CAN bit timing calculator for 500kbps nominal and 1Mbps data and it gives me


i can confirm that they are being set in the registers .. I've tried a few other calculators and tried some other setting but i only seam to get data at 125kbps NOT 500kbps. I'm hoping that i've not set something as i'm new to the micro.
Any guidance I'd be most grateful ...
I'd also like to know if i can turn off the Extended ID as i cannot see the setting
i did originally start with the normal CAN in syscfg but when i selected my messages it crashed on me ....
Thanks