Part Number: TMS320F28384D
Dear Madam/Sir,
I have a requirement of 7 UART channels in my overall application. As per the datasheet the above chip supports 4 SCI channels ,one CM-UART
For debugging purpose, generally we use one of the SCI- UART with FTDI chip interface and connect with Host. But I dont want to waste one of the UART for this purpose.
What is the alternative approach? Can I use USB of the TMS 320F28384D chip for this purpose? kindly clarify.
And also what is the function of FSi_Rx mode ? Is it work similar to UART channel? Kindly clarify. I am a bit struck as I was not able to finalise the number of channel requirements.Also suggest me what best can be done?
Pl clarify , is there any application note to understand the performance computation of the overall dual core in case of utilizing this many serial channels.
Thanking you ,
-
1
USB
How to connect for debugging ?????
2
SCI port
To interface with BEL System
3
SCI Port
To send the data between System Controller to BARCO Monitor
4
SCI port
To interface Range Controller
5
SCI port
To interface with Vehicle controller
6
CM UART shall be used
Integrated Sight Package
7
FSI- RX MODE
HOW TO USE IT?