Part Number: TMS320F28388D
Hello,
I want to know if it is possible to trigger multiple CLA Tasks like Task 1 and Task 2 with same interrupt source like ADCAINT1. If both the tasks are configured with the same interrupt source, will the CLA execute Task 1 and Task 2 in order or it will only execute Task 1 and will not execute Task 2?
Regards,
Ram Alla.