This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388S: Not able to flash the code

Part Number: TMS320F28388S

Hi,

I mistakenly programmed the Z1OTP_CSMPSWD0 and Z1OTP_CSMPSWD1 registers due to which I am not able to erase and flash the code through CCS. Below error I am getting while flashing the code:



Also, if I am flashing the code through CCS using On-Chip Flash by giving below changed password then erase and flash both are working fine, but not working without using On-Chip Flash.

Can you please suggest the changes which will resolve this error?

Thanks in advance,

Deepankan