This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: TMS320F280025C, EPWM, Only use A side

Part Number: TMS320F280025C

Hello.
Please forgive my poor English notation.

I am using the ePWM function of the TMS320F280025C to generate PWM waves with variable duty ratio.
So, is it possible to disable the B side (EPWMxB) when all I want to use is the A side (EPWMxA)?
If it is possible, how do I set it up using the .syscfg file?

  • Hi,

    Thanks for contacting the E2E forums!

    Yes, definitely you can do that. Please don't configure the action qualifier for EPWMxB. You won't see any output on the B terminal. Also, make sure that the dead band is disabled.

    This should give you the desired output waveform.

    Thanks,

    Aditya