This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: internal 1.2V LDO power dissipation, recommendation for external 1.2V switching power supply

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: TPS74801-Q1, TPS7A88-Q1

Hi all,

looking at the max power consumption for the heavy load from the datasheet, for VREG enabled vs VREG disabled, it looks like there is approx 700mW dissipated in the internal LDO, which is a pretty high number.

Do we generally recommend to use an external supply for the 1.2V supply?

For efficiency reasons, is there a TI switching power supply part we can recommend for the 1.2V supply?

We see the voltage tolerance for the 1.2V rail in the datasheet. Is there a ripple requirement on this rail, so we can check on for an appropriate switching power supply?

Thanks!
--Gunter