Part Number: TMS320F280039
Hi Team,
Good day!
Customer just reported to me today from their factory that they are facing concern regarding F280039CSPM MCU flash memory.
There were instances where the firmware loaded onto the MCU flash memory either becomes erased or the data in a section becomes altered.
- The MCU programming is done after AI SMT stage, prior to MI wave solder.
- MCU is de-energized after initial programming, then 3.3V is re-applied and flash memory contents checked.
- The board is then subjected to wave solder, with a maximum solder temperature of 2630C.
- The assembled unit is then loaded to T1 station, where in some instances it would not power-up or communicate at all due to MCU “program corrupted”.
Kindly advise on any potential effects on MCU flash memory when subjected to up to 2630C wave solder temperature environment.
The only item I found on the datasheet is possible INTOSC frequency shift due to reflow (section 6.12.3.5 page 97).
Thanks!
BR,
Alfred