Hi Team,
I am working on a sine wave single-phase inverter (300-400DC to 220-50HzAC) which is using F280049C MCU of TI.
During inverting, I want to control the rising of an AC voltage
let's say, for an initial 1 sec(some time), AC voltage should be at 25% of 220V after 1 sec, it should be at 50% of 220V, then 75% & then 100%.
.I am looking for the sample code and reference design for the same.