This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386S: Does the CMPxHR has to be used in conjunction with DBxEDHR?

Part Number: TMS320F28386S

Hi TI Experts,

I need to generate a pair of PWM signals with high resolution of duty cycles, which are used in a half-bridge converter. The deadband does not need to have high resolution. However, I am not sure if the generated PWMs have high resolution if the CMPxHR is enabled while the DBxEDHR is disabled.

Best regards~