Part Number: TMS320F28027F
Other Parts Discussed in Thread: DRV8353RS-EVM, MOTORWARE, DRV8301, DRV8353, DRV8305, BOOSTXL-DRV8323RS, BOOSTXL-DRV8323RH
Followed the guide (SLVUBH8B) on the DRV8353RS-EVM to run the operation.
GUI was executed through motorware. The guide says to install via DRV8353Rx-1.0.0-window-installer, but I couldn't find the file, so I installed version 1.0.1.

When I checked through other people's question history, they said that the variable called gDeviceVariant is declared in the
file called proj_lab05b.c. The variable called gDeviceVariant is not declared in the file I downloaded. So I arbitrarily declared gDeviceVariant = 0xFF.
In addition, the guide says that there is a code that can run the DRV8353 GUI, but when I checked the code, there is only a code that enables DRV8301 and
DRV8305.

Did I install the program wrong?
When I asked the Motor Driver Forum, they said it would be a good idea to contact the C2000.
And can I run InstaSpin-MOTION with DRV8353?
I've searched for that method, but there's no guide.