Part Number: TMS320F2800152-Q1
Dear Champs,
1. If the GPIO pin is overcurrent, will it cause the DSP to reset?
2. If the GPIO pin output is low level, but an external high level is given, will it cause the device to reset or work abnormally? Does this ultimately depend on the size of the pin sink current?
3. According to the specification, the source/sink current capability of is 4mA. Is this value related to the temperature? What is the relationship between the amount of sinking current that can be tolerated and the time it can withstand it?

Thanks!
Best Regards,
Julia