Other Parts Discussed in Thread: DRV8353, LAUNCHXL-F2800157, DRV8353RS-EVM
Hello team,
I am working on the position control of the 48V ABZ+PWM motor using F2800157 launchpad with DRV8353 power board using encoder feedback. I am using the TI Universal motor code (UMC) and I have enabled the macros related to the motor encoder. After enabling MOTOR1_ENC motor is running without encoder feedback and its running in a constant speed irrespective of the motorVars_M1.speedRef_Hz value.
Previously I have tested for the HALL feedback and MOTOR_FAST method with using the F2800157 launchpad and DRV8353 MOSFET board with current and voltage feedback, its working fine and I am able to change the speed in both directions.
- Kindly help for the above issue and whether I need to change anything in the UMC to run the 48V PWM+ABZ motor with the encoder feedback compared to the MOTOR1_FAST method.
Thanks and Best Regards,
Kirana H P