Other Parts Discussed in Thread: C2000WARE
Hi:
how to compute crc16-x25 with vcrc?
Could you provide some examples?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
how to compute crc16-x25 with vcrc?
Could you provide some examples?
Part Number: TMS320F280039C
How to use VCRC to implement CRC16 X25 check.
--
Thanks & Regards
You can refer to the example 28003x_vcrc_crc_16 in C2000Ware.
CRC16 X25 requires the inputs to be reflected (use CRC_run16BitPoly2Reflected(), which corresponds to the required polynomial 0x1021 and reflects the inputs before feeding them into the CRC compute), the output to be reflected, and XORd with FFFF.
Thanks,
Sira