Part Number: TMS320F28388S
Other Parts Discussed in Thread: LP-XDS110, CCSTUDIO
Hi, I have a board that we designed with TMS320F28388S Microcontroller. I am powering it up with 3.3 Volts, and forgot to add the 1.2 Volt, as i am more familiar with the new C2000 Mcu's, which has internal VREG to convert 3.3 to 1.2 Volts. So i made a small LDO board that use to generate 1.2 Volts and supply it to the MCU 1.2 Volt core.
But the microcontroller is not getting detected by the MCU. When i probed the MCU reset pin, i found out it getting resetted after 14.6mS and for 46uS(keep low for 46uS and then goes high,but after 14 mS again goes low for 46uS).
I have attcahed the circuit, please review it, and let me know the possible reasons. Redefined.pdf
I am using internal crystal, no external crystal onboard.