Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello Team,
actually, SPI DMA support 16 bit or 32 bits. I'm using SPI support controller which support 8-bit commands.

frame format like this.
void InitSpi(void)
{
// Initialize SPI-A
// Set reset low before configuration changes
// Clock polarity (0 == rising, 1 == falling)
// 16-bit character
// Enable loop-back
SpiaRegs.SPICCR.bit.SPISWRESET = 0;
SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;
SpiaRegs.SPICCR.bit.SPICHAR = (8-1);
// SpiaRegs.SPICCR.bit.SPILBK = 1;
// Enable master (0 == slave, 1 == master)
// Enable transmission (Talk)
// Clock phase (0 == normal, 1 == delayed)
// SPI interrupts are disabled
SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;
SpiaRegs.SPICTL.bit.TALK = 1;
SpiaRegs.SPICTL.bit.CLK_PHASE = 1;
SpiaRegs.SPICTL.bit.SPIINTENA = 0;
// Set the baud rate
//SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = SPI_BRR;
SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = 4;
// Set FREE bit
// Halting on a breakpoint will not halt the SPI
SpiaRegs.SPIPRI.bit.FREE = 1;
// Release the SPI from reset
SpiaRegs.SPICCR.bit.SPISWRESET = 1;
}
I done SPI configurations like this.
please give me any suggestion, o resolve this issue.