Part Number: TMS320F28388D
Hi experts,
In our current design we use the TMS320F28388D with two ethercat interfaces. Our customer wants now a ethernet service interface. We are using the version
HLQFP (PTP) | 17, is it possible to use two ethercat ports and 1 ethernet port togheter with this chip?
I checked the pins and
| ESC_PHY1_LINKSTATUS | ENET_MII_INTR |
is both on GPIO68. And
| ESC_LED_LINK0_ACTIVE | ENET_MII_TX_CLK |
is both on GPIO58.
Is it possible to handle this and have all three interfaces in one ? Or is only possibility to go to the TMS320F28388DZWTS?
Thank you!